Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Product List
Migrating from 8/16-bit MCUs to 32-bit ARMs Slide 12
The prefetch buffer is constantly in use. As shown above, the instructions are stored in the Pre Fetch Buffer (PFB) and supplied to the processor from here.  Another speculative fetch begins as the ARM core is executing from the PFB and this data gets loaded into the data latch.  As soon as the last instruction in the Quad is executed, the data is transferred to the Pre Fetch buffer and the process starts again.
PTM פורסם ב: