Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Product List
Migrating from 8/16-bit MCUs to 32-bit ARMs Slide 14
The PFB and the Data bypass do everything they can to speed up access to Flash, but branch operations are tougher to handle. The non-sequential address of the a branched instruction is going to require a full Flash Access Cycle unless it has been branched to previous instructions – which is common in the case of loops. This branch target is stored in the Branch Trail Buffer and can significantly increase performance in certain types of code with branches.
PTM פורסם ב: