Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Product List
Migrating from 8/16-bit MCUs to 32-bit ARMs Slide 30
Handling these interrupts is the responsibility of the Vectored Interrupt Controller, or VIC. The VIC is implemented based on an IP block also licensed from ARM – these standard IP blocks are known as PrimeCells and are commonly found in many vendors’ implementations of ARM cores. The VIC has 32 IRQs, where 16 of them can be auto vectored. This class of interrupts, known as Fast Interrupts, are a higher priority of interrupts for the core to respond to. Note that in the LPC2300 and LPC2400, an advanced VIC has been implemented allowing for a full 32 fast interrupts!
PTM פורסם ב: