Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Product List
Migrating from 8/16-bit MCUs to 32-bit ARMs Slide 34
This slide shows all of NXP’s currently released ARM solutions as well as several that are soon to be released to production. Note the range of package options, onboard memory sizes, peripheral mix, and range of features. Also, within each package type and size, there is a universal pin-out – allowing, for example, use of the LPC213x devices on the same layout as the LPC214x devices. For instance, USB could be provided in a design using the LPC214x along with a differentiated, lower-cost product without USB using the LPC213x – and use the same layout!
PTM פורסם ב: