Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Real Time Clocks Slide 12
In order to increase accuracy, an electronic tuning register has been included in the PCF2123. It can be used to compensate for the aging of the quartz crystal, temperature compensation, and initial accuracy tuning. The correction is made by adding or subtracting pulses from an internal 64 Hz clock and is made once every two hours in normal mode or once ever hour in course mode.
PTM פורסם ב: