Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Real Time Clocks Slide 4
In the diagram on this slide, the microcontroller is still the heart of the system, but is supported by a separate RTC. A stand-alone RTC can achieve higher accuracy and/or lower power consumption than an integrated RTC. Usually an integrated RTC will not have temperature compensation while some stand-alone RTCs have temperature compensation in order to achieve high accuracy. Due to the use of an optimal process for RTC construction, current consumption can be very low.
PTM פורסם ב: