Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Real Time Clocks Slide 13
These are some of the potential automotive applications for RTCs. In navigation systems, keeping time when the navigation is switched off allows for a faster restart when the navigation system is switched on again. Certain countries have legislation to avoid truck drivers from working too long hours, which would increase the accident risk. A tachograph can be used to record vehicle speed and whether the vehicle is stationary or not. An RTC can provide superior accuracy and low power consumption for tachograph devices. RTCs can also be used in hybrid cars to manage battery power and in electronic road pricing systems to record accurate time references and time stamps. All modern cars are equipped with on board diagnostics, which required accurate time stamping of certain events.
PTM פורסם ב: