Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List Associated Content
Global Support

RIIM™ is compliant to EN 300 220, the 868 MHz band in Europe, and is pre-certified for FCC CFR47 Part 15.249, the 915 MHz band in the Americas. The IPM module is software configurable and the remaining hardware can typically cover both 868 MHz and 915 MHz. This allows a RIIM network to operate in the orange and grey regions on the map. The 915 MHz frequency is allowed in most of North and Latin America, and half of South America. The 868 MHz is allowed in Europe and many countries in Asia and Africa. The light beige regions, including Brazil and India, follow other regulations. Those regulations are technically possible to support with RIIM, but are not implemented in the standard offering: contact Radiocrafts for support. The information for the black regions were not available at Radiocrafts at the time when this map was created.

PTM פורסם ב: