Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List Associated Content
Industrial Grade Quality

Since the foundation of Radiocrafts, the company has been focused on industrial applications with high quality. This shows in the way Radiocrafts builds on proven solutions and adapts the solution for high reliability. The performance is also adapted to the reliability requiring industrial applications, the frequency hopping with 6TSCH helps to find the noiseless channels and the 700 m range in urban environments translates to coverage in large industrial sites with good margins. On another angle, 100% of the modules shipped from Radiocrafts are tested on the RF level, ensuring high quality for each individual module. This process has resulted in an exceptionally low number of hand-backs for the two million plus modules shipped and great customer satisfaction all over the world.

PTM פורסם ב: