Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List Associated Content
Over the Air (OTA) Updates

Over the Air (OTA) updates make it possible to update RIIM™ in the field. OTA can save on large costs compared to sending out installation staff to upgrade network nodes with bugs that are already installed in the field, and it can also be used to add or modify the local data processing needed for changes in the environment.

PTM פורסם ב: