Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
AECLOUD-Slide10

The AE-CLOUD2 kit includes the Renesas Synergy™ S5D9 microcontroller board, at the core of the board.The board includes on-board sensors such as the Renesas Digital Ambient Light Sensor, as well as sensors for microphone, environmental, accelerometer, and magnetometer. These sensors have been labeled on the PCB board for each identification and location. The board has a built in Ethernet PHY chip and Ethernet port and is expandable via the Grove, PMOD, and Arduino headers on the board. While the S5D9 board has an on-board debugger, the JTAG connector provides the option for a developer to connect an external debugger if they so choose.

PTM פורסם ב: