Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
AECLOUD-Slide19

The AE-CLOUD2 supports connectivity options for Cellular, Wi-Fi, and Ethernet. The three connectivity options can be connected to the S5D9 Microcontroller board as shown in the picture. All three connectivity options can be connected at the same time allowing a developer to switch between the connectivity options or design applications with a primary and back connectivity option.

PTM פורסם ב: