Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
AECLOUD-Slide16

Using a single BG96 module, AE-CLOUD2 supports multiple cellular standards, as well as a GPS receiver that enables the prototyping of position tracking applications. This table describes the global frequency support of AE-CLOUD2. The 3GPP is the standards organization responsible for defining the protocols and RF spectrum use for cellular technologies. AE-CLOUD2 also supports EGPRS which can be used if CAT-M1 or CAT-NB1 is not supported in a developer’s region or as a backup cellular connectivity option in case CAT-M1 or NB-IoT fail. With support for various cellular frequencies and technologies, the AE-CLOUD2 reference design can work anywhere in the world regardless of the protocols supported by the local carrier.

PTM פורסם ב: