Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
AECLOUD-Slide25

The Cloud Toolbox demo allows the customers to use the Synergy MQTT and TLS integrations to connect to Microsoft, Amazon, Google, or the cloud vendor of choice. The customer can quickly and easily compare connecting using Cellular, Ethernet, or Wi-Fi which are supported by the Synergy Software Application frameworks. The customer can also visualize the sensor data on a private web dashboard that is password protected and use the web dashboard source code to integrate the Cloud Toolbox with ones own cloud account.

PTM פורסם ב: