Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Slide 68 Slide 69 Slide 70 Product List
Electromagnetic Noise Reduction Slide 39

At high frequencies, the bus lines are signal transmission channels. Impedance mismatches at the ends of these channels can cause ringing – a form of noise – at a frequency corresponding to double the signal round-trip time. A 20 cm signal line will have a 250MHz ringing frequency, for example, since the period of the wave is 4nsec. The traditional method for eliminating unwanted reflections in a transmission channel is to dissipate the energy. You can do this by adding damping resistors in series with the lines from the output buffer, as shown here. You might be able to use a resistance value as large as 5kΩ, but be aware that if the value is too high, it can cause various types of subtle failures. Alternatively, you can insert a terminating resistor to ground at the receiving device. Adding the damping resistor is generally a better solution, though, because when you use a terminating resistor, you can get either excessively high voltage at the output buffer, or inadequate input current at the receiver because the Thevenin termination has been changed. Above all, remember that if you keep the transmission channels short compared to the signal wavelength, there will be minimum ringing, so no damping resistors will be required.

PTM פורסם ב: