Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Slide 68 Slide 69 Slide 70 Product List
Electromagnetic Noise Reduction Slide 59

Another very effective IC design technique engineers can apply is to arrange the Vcc and GND terminals on the package in an optimum way, quite close to one another. The resulting pin layout of the package will make it easy to mount bypass capacitors near and directly across those terminals, where they will be most effective in reducing noise emissions from the microcontroller. Additionally, if the MCU designers can make the wiring of the signal lines parallel inside the package and on the semiconductor chip, they can build into the microcontroller effective noise filters that are comprised merely of wiring inductance and parasitic capacitance.

PTM פורסם ב: