Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Slide 68 Slide 69 Slide 70 Product List
Electromagnetic Noise Reduction Slide 55

A third technique is to optimize the output impedance of the buffer in the MCU to the wiring of the circuit board on which the microcontroller will be mounted. Since the wiring pattern of a two-layer printed circuit board itself has an impedance of approximately 150 to 200 Ohms, the impedance the buffer has to drive will be 100 to 150 Ohms when the system components to which it connects are surface mounted. BY designing the output impedance of the buffer to be in the 100 to 150 Ohms range, the MCU designers can control waveform ringing and reduce unwanted radiation.

PTM פורסם ב: