Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Slide 68 Slide 69 Slide 70 Product List
Electromagnetic Noise Reduction Slide 60

This page highlights some of the noise-related development that went into the design of the M16C series MCUs. It also shows a practical example of the design techniques we just mentioned. Specifically, it points out the innovative pin layout of the Renesas devices, and, especially, the circuit board implementation pattern of Vcc, GND, and the oscillation circuit. The M16C microcontroller’s pin layout is the result of careful analysis and prudent, insightful, design. The power-related pins are arranged to prevent power-line short circuits: XOUT, the GND (Vss), then XIN, the VCC. This arrangement simplifies connection to the 2-terminal oscillation circuit and places the ground pin between the oscillator pins.

PTM פורסם ב: