Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Target Application

Based on the five features of RX140, these are the applications suitable for RX140 usage. As the RX140 inherits RX130 peripheral functions, it can continue to be used in the consumer electronics field. In addition, with CANs and Security installed, these functions are used in the BAs and IAs.

PTM פורסם ב: