Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Comparison Of Functions For Different Packages 1

Here is another slide included for reference. This type of chart will be familiar to those who have read through a user’s manuals. Here, users can easily see the trade-offs in features and package sizes for both the 64 KB and 256 KB devices. Also, on this chart is the package lineup that differs between the two Flash sizes. The smaller 64 KB part will offer the smaller 32-pin QFP and QFN packages, while the 256 KB will add an 80-pin QFP package.

PTM פורסם ב: