Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Product Overview 1

This diagram summarizes the outline of RX140 products. It will focus on the distinctive specifics of RX140. The CPUs feature RXv2 cores to deliver the best throughput capabilities in RX100 series. Power supply voltage is available from 1.8 V to 5.5 V. The accuracy of the high-speed on-chip oscillator is improved to ±1.0% error. The wakeup time has been accelerated, and when using the high-speed on-chip oscillator, the operating state can be restored at 6.2 μs. It is equipped with a peripheral function like that of the RX130. Specifically, peripheral functions such as communication, timers, and analog are equipped with the same modules and channels as RX130. It is equipped with a new-generation capacitive touch sensor (CTSU2SL, CTSU2L) as a peripheral function improved by RX140. A new feature is RCAN x 1ch. In addition, RX100 series is equipped with the first hardware security. Specifically, it includes a cryptographic accelerator (AES) and an authentic random number generator (TRNG). The package line-up includes LFQFP ranging from 40 pins to 80 pins, 32 / 64-pin of LQFP and 32 / 48-pin of HWQFN.

PTM פורסם ב: