Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
freq op
These are the three common output types that are offered with the LP35. With a known resolution and rotational speed (RPM), the customer can use the performance graphs to determine the maximum allowable cable length. Each has their own operating parameters. The most common type specified is the 28/V, followed by the 28/5 and the 28/VR. The driver should be consistent with the planned operating scenario.
PTM פורסם ב: