Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
reliable res
The Magnetic technology that the LP35 uses is in the “sweet spot” between durability and resolution. It performs at a level where 95% of encoder applications fall into for resolution and reliability. With almost double the bearing life of optical encoders, the LP35 excels in applications that bang up the encoder through constant usage like Light Rails and Logging Equipment.
PTM פורסם ב: