Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
hi perf valid
This test validates that using the multipole magnetic ring technology results in an absolute position error, or overall accuracy of +/- 0.1°. Note that the results are very repeatable and the error is not cumulative. This level of accuracy can be visualized as hitting an 18” diameter target (the size of a basketball hoop) from a distance of one-half mile.
PTM פורסם ב: