Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
CP21xx USB Bridge Slide 14

As mentioned, the CP2112 uses the HID class drivers like the CP2110. Remember, the HID class driver is part of most operating systems. In order to use the HID class for the host application most often developers need to download the Windows DDK. With the Silicon Labs solution, a library is provided that encompasses the HID API and the Windows DDK is not required. Two application notes for the development flow using the HID class are provided. The first is AN495 with covers the report formats for the data that is bundled in the USB frames. The second application note (AN496) defines the API functions used by the host application to transfer data to the device.

PTM פורסם ב: