Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
CP21xx USB Bridge Slide 15

Shown here is a copy of a function from the CP2112 host application used to retrieve data from the device. These are example API calls available in the library provided. The highlighted example is used to get the device part number and illustrates how a developer could use the API in their own application.

PTM פורסם ב: