Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
CP21xx USB Bridge Slide 16

The CP2112 device bridges data between USB and SMBus\I²C. Silicon Labs provides example applications to highlight the operation of the device. The HIDtoSMBus\I²C Example application highlights the operation of the API functions. For example, the Data Transfer tab in the GUI provides the ability to transfer data between the host and an SMBus\I²C slave device. The steps shown here illustrate how to use the tool. The slave address can be entered and the data transferred using the Read Request, Get Read/Write Transfer Status, Read Response and Force Read Response API buttons. Each of these buttons have a corresponding API call defined in AN496.

PTM פורסם ב: