Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
CP21xx USB Bridge Slide 3

One method used to bridge the com port data is to use a custom driver that gets installed prior to using the bridge. This method is the easiest to use since there are no host side application modifications required. From a software perspective there is no difference between the Virtual Com Port (VCP) and a standard com port. The VCP driver method does require an installation step since these drivers are not part of the operating system. Silicon Labs provides a VCP driver that can be freely downloaded and distributed.

PTM פורסם ב: