Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Solves Bidirect

The Si860x bidirectional isolators also offer a significant size savings compared to optocoupler solutions. In addition, the Si860x family has configurations available which include several unidirectional data channels in addition to the bidirectional channels. A use case for this arrangement of channels would be an I2C bus connection which also requires an interrupt (INT) or reset (RST) signal (both unidirectional). This feature is unique to Skyworks Solutions and means that a complete solution can be 33% smaller than the multi-device offerings from competitors.

PTM פורסם ב: