Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
C8051F38x USB MCU Slide 23
The registers used to define which addresses are recognized by the hardware are the SMBus slave address register and the SMBus slave address mask register. A single address or range of addresses (including the general call address 0x00) can be specified using these two registers. The most-significant seven bits of the two registers are used to define which addresses will be ACKed. A 1 in bit positions of the slave address mask SLVM[6:0] enable a comparison between the received slave address and the hardware’s slave address bits. A 0 in a bit of the slave address mask means that bit will be treated as a “do not care” for comparison purposes. In this case, either a 1 or a 0 value are acceptable on the incoming slave address.
PTM פורסם ב: