Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
C8051F38x USB MCU Slide 7
The default state of the registers of the C8051F38x family places the device in the same operating state as the previous family. Therefore, the firmware from the C8051F34x will run on the C8051F38x devices unmodified. One example is the clock multiplier settings. In the previous family which used the clock multiplier to generate the 48 MHz, the multiplier had to be set up and stable. The MUX settings in the chip were then set to drive the 48 MHz to the system clock and the USB clock. In the C8051F38x family this same code can be used and the register settings will cause the 48 MHz internal oscillator to drive the nodes as the output of the clock multiplier did.
PTM פורסם ב: