Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Magnet Technology and Their Uses Slide 17

The Curie temperature of a magnet or ferromagnetic material is that temperature where the magnetic properties are lost. The temperatures are usually quite high. However, they can and are reached in several applications. In many cases, once the temperature drops below its Curie temperature, the magnetic properties return. This is the case with ferromagnetic materials or some magnets may lose some or all of their magnetism.

PTM פורסם ב: