Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Magnet Technology and Their Uses Slide 22

There has been much speculation about large magnetic fields physically distorting reed switches when the magnetic fields are brought into the proximity of a reed switch or reed switch sensor. In fact, the tiny nickel/iron ferromagnetic blades will reach a magnetic saturation point and increasing the external magnetic field will have no effect on the reed blades. One can use the analogy of filling a glass of water. Once it is full, no matter how much more water users try to pore into the glass, it will not accept any additional water.

PTM פורסם ב: