Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Magnet Technology and Their Uses Slide 27

When power is applied to the reed relay coil, the magnetic field produced must be at least equal and opposite in polarity of the magnet. The oppositely polarized magnetic field produced by the coil will open the contacts. Removing the coil power will cause the contacts to automatically reclose. This completes the cycle of how a normally closed reed relay works. What is so effective about a normally closed reed relay is that the relay will draw no power for applications calling for the contacts to be closed for long periods of time. A latching reed relay is accomplished in a similar way but generally uses two coils. The first coil closes the contacts and the second coil opens the contacts.

PTM פורסם ב: