Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
Magnet Technology and Their Uses Slide 23

Not only is magnetism available in nature and available via man-made magnetic compounds, but it can also be generated via an electromagnet. This is generated by winding copper into a cylinder and passing a current through the wire. A uniform magnetic field is generated in the center of the cylindrical coil. The stronger the current is, the stronger the magnetic field will be.

PTM פורסם ב: