Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Reed Sensors vs Hall and Electromechanical Slide 10

Both the reed sensor and the Hall sensor are activated by an external magnetic field; however, electromechanical sensors require a mechanical movement that presses into a mechanical lever mounted external to the sensor. This lever will directly close a set of contacts usually internal to the sensor packaging. The sensor can have two or more leads exiting the packaging for direct load switching. These sensors can have single pole single throw (spst), single pole double throw (spdt), and double pole double throw (dpdt) lead configurations.

PTM פורסם ב: