Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Reed Sensors vs Hall and Electromechanical Slide 7

The hall sensor is a semiconductor device which is made using an integration process. An electric current must be flowing into the device in order to carry out its function. With current flowing, the hall sensor will interact with the presence of a magnet field producing a voltage. This voltage level, measured in milli-volts, is proportional to the relative strength of the magnetic field.

PTM פורסם ב: