Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Reed Sensors vs Hall and Electromechanical Slide 4

A reed sensor is comprised of a small hermetically sealed glass cylinder usually sealed and packaged in plastic or metal having two leads that directly provide a switching function. Reed sensors come in hundreds of different sizes and shapes suitable for a variety of applications. The sensitivity to closure is measured in milli-tesla (mT) or ampere turns (AT). The reed sensor typically uses an external magnet to close the contacts. When the magnet is brought close enough to the reed sensor, the contacts will close or pull-in (PI). Withdrawing the magnet, the contacts will open or drop-out (DO). Hysteresis is another useful parameter. Hysteresis is just the ratio of the pull-in divided by drop-out (PI/DO).

PTM פורסם ב: