Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Gate Drivers Overview Slide 11

The interlocking feature is a little bit different. This slide shows the truth table of the L6390. If LIN and HIN enables both gates at the same time, a short circuit occurs between the DC bus and ground. To avoid this short circuit, the interlocking feature turns OFF the gate drivers when the application tries to turn the gates ON at the same time. In some power supply applications, both gates must be turned ON at the same time, so this function is not always integrated.

PTM פורסם ב: