Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Gate Drivers Overview Slide 9

The dead time is basically the elapsed (or delay) time before a gate can be turned ON after the other gate was turned OFF. If a gate is turned ON before the other one is completely turned OFF, a short circuit between the DC bus and the ground is possible. To avoid this problem, a dead time forces the two bridges to be OFF for a given period of time.

PTM פורסם ב: