Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Gate Drivers Overview Slide 3

The choice of monolithic solution or gate driver is going to be mostly determined by the voltage and current. Below 50 V and 3 A, a monolithic solution can be used. In a monolithic device everything is in the same die and the bridges are directly connected with the MOS on the die. Above 50 V or 3 A, the monolithic technology does not satisfy the requirement. In that case, it is necessary to select gate drivers. High-voltage gate drivers in half-bridge configuration are available to 600 V, above that the customer will need to select from single gate drivers with isolation. The focus of this tutorial is on the half-bridge gate drivers.

PTM פורסם ב: