Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Gate Drivers Overview Slide 14

A key issue with high voltage gate drivers is the below ground phenomenon. When the high side is turned OFF, a negative voltage appears on the OUT pin. This can destroy the gate driver if it is not robust enough. The amplitude and the duration depends on various parameters of the design, like the load, but also the parasitic elements of the PCB.

PTM פורסם ב: