Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
VL6180X FlightSense Slide 15

The graph here shows the VL6180X ALS spectral response. As shown in the graph, the ALS response is photopic meaning it is closely matched to the human eye response. It is important to note that the ALS test data shows a maximum of 6% illuminance error with different types of gain settings and with different lighting sources.

PTM פורסם ב: