Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
VL6180X FlightSense Slide 27

In summary, the VL6180X is STMicroelectronics’ first proximity sensor based on time of flight technology. Compared to conventional IR, which is typically used in the market today, the VL6180X actually measures distance. The VL6180X also has an ambient light sensor (ALS) included that can detect light as low as 1 Lux and as high as 100 K Lux.

PTM פורסם ב: