Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
VL6180X FlightSense Slide 17

This slide shows the VL6180X module. It is a 12-pin device with package dimension of 2.8 X 4.8, 1 millimeters high. As shown on the slide, on the left-hand drawing, starting from left to right, the smallest hole is the sensing area, and next to it is the ambient light sensing area. The next mark, is a manufacturing process plastic gate marking. All the way to the right, is the IR light source emission aperture. The VL6180X part is an QFN reflow-able. The reflow profile that should be used with the VL6180X is located in the datasheet found on ST.com.

PTM פורסם ב: