Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
WiFi Modules Overview Slide 5

Shown here is a block diagram from ST on the IoT. The typical IoT product is going to have in some way, shape, or form a lot of these blocks in it. This includes a microcontroller in some form, some type of a user interface, connectivity, it may require protection depending on how it is exposed to the environment, and significant power management. Most IoT devices are geared toward low power, battery powered type applications. Sensors, including: pressure sensors, temperature sensors, accelerometers, gyros. Everything ST makes from the digital sensor standpoint fits very well into the IoT. Additionally, analog sensors, like MEMS microphones, and then analog front end-type devices, all signal transducers and switches. This block diagram illustrates that ST can provide a full system solution with their line card.

PTM פורסם ב: