Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
WiFi Modules Overview Slide 7

All of the embedded modules follow the same plan: a host microcontroller at the designer’s end hosting the application and then talking via UART to the module itself and then either 2.4 GHz or in the case of the sub-Gigahertz and other devices, 915 or in Bluetooth 2.4 GHz also. It is a serial-to-RF application, so in most cases the entire application interface in the stack are all on the module.

PTM פורסם ב: