Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
WiFi Modules Overview Slide 14

These modules are FCC, IC, and CE certified, so they are good for Europe, USA, and all countries that follow those requirements. ST also has ANATEL certification for South America, mainly for Brazil and other countries that follow ANATEL certification that is beginning to be implemented. The communication to the module is over AT command set through UART. There are two different system modes. There is the mini-access-point mode and the station mode. It has sockets, web server capability and REST API commands that will be discussed. As mentioned before, it has TLS 1.2 and SSL 3.0 for end-to-end security. Certain modules have over-the-air update firmware capabilities and they all provide easy provisioning, which will also be discussed. Additionally, it has up to 18 dBm output power.

PTM פורסם ב: