Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
WiFi Modules Overview Slide 16
The modules come with a full AT command based software stack. Within that, the software package will give users a .bin file that can be downloaded to the module direct via UART, an .ota file, which is a slightly different configuration that can be downloaded over the air, and the change logs and license file. There are two different versions: the 001 is for the .11 family and the 002 software package is for the .21 family, so users will want to make sure they load the proper firmware package.
PTM פורסם ב: