Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Thermally Conductive Gap Filler Rolls Slide 27

T-Global LI series is a line-up of highly thermally conductive adhesive tapes that can be used for the attachment of heat sinks and other components when thermal management is a requirement in addition to mechanical adhesion. The LI series of tapes are proven to offer excellent reliability when exposed to thermal, mechanical, and environmental conditioning. They are offered in a variety of configurations, as detailed in the typical properties table. All of the products in this series are available in standard sheets, as custom cut die-cuts, and on rolls.

PTM פורסם ב: